Warnings are diagnostic messages that report constructions which are not inherently erroneous but which are risky or suggest there may have been an error.
The following language-independent options do not enable specific warnings but control the kinds of diagnostics produced by GCC.
-fsyntax-only-fmax-errors=n-w-Werror-Werror=The warning message for each controllable warning includes the option which controls the warning. That option can then be used with -Werror= and -Wno-error= as described above. (Printing of the option in the warning message can be disabled using the -fno-diagnostics-show-option flag.)
Note that specifying -Werror=foo automatically implies
-Wfoo. However, -Wno-error=foo does not
imply anything.
-Wfatal-errorsYou can request many specific warnings with options beginning ‘-W’, for example -Wimplicit to request warnings on implicit declarations. Each of these specific warning options also has a negative form beginning ‘-Wno-’ to turn off warnings; for example, -Wno-implicit. This manual lists only one of the two forms, whichever is not the default. For further, language-specific options also refer to C++ Dialect Options and Objective-C and Objective-C++ Dialect Options.
When an unrecognized warning option is requested (e.g., -Wunknown-warning), GCC will emit a diagnostic stating that the option is not recognized. However, if the -Wno- form is used, the behavior is slightly different: No diagnostic will be produced for -Wno-unknown-warning unless other diagnostics are being produced. This allows the use of new -Wno- options with old compilers, but if something goes wrong, the compiler will warn that an unrecognized option was used.
-pedanticValid ISO C and ISO C++ programs should compile properly with or without this option (though a rare few will require -ansi or a -std option specifying the required version of ISO C). However, without this option, certain GNU extensions and traditional C and C++ features are supported as well. With this option, they are rejected.
-pedantic does not cause warning messages for use of the
alternate keywords whose names begin and end with ‘__’. Pedantic
warnings are also disabled in the expression that follows
__extension__. However, only system header files should use
these escape routes; application programs should avoid them.
See Alternate Keywords.
Some users try to use -pedantic to check programs for strict ISO C conformance. They soon find that it does not do quite what they want: it finds some non-ISO practices, but not all—only those for which ISO C requires a diagnostic, and some others for which diagnostics have been added.
A feature to report any failure to conform to ISO C might be useful in some instances, but would require considerable additional work and would be quite different from -pedantic. We don't have plans to support such a feature in the near future.
Where the standard specified with -std represents a GNU
extended dialect of C, such as ‘gnu90’ or ‘gnu99’, there is a
corresponding base standard, the version of ISO C on which the GNU
extended dialect is based. Warnings from -pedantic are given
where they are required by the base standard. (It would not make sense
for such warnings to be given only for features not in the specified GNU
C dialect, since by definition the GNU dialects of C include all
features the compiler supports with the given option, and there would be
nothing to warn about.)
-pedantic-errors-Wall-Wall turns on the following warning flags:
-Waddress
-Warray-bounds (only with -O2)
-Wc++0x-compat
-Wchar-subscripts
-Wenum-compare (in C/Objc; this is on by default in C++)
-Wimplicit-int (C and Objective-C only)
-Wimplicit-function-declaration (C and Objective-C only)
-Wcomment
-Wformat
-Wmain (only for C/ObjC and unless -ffreestanding)
-Wmissing-braces
-Wnonnull
-Wparentheses
-Wpointer-sign
-Wreorder
-Wreturn-type
-Wsequence-point
-Wsign-compare (only in C++)
-Wstrict-aliasing
-Wstrict-overflow=1
-Wswitch
-Wtrigraphs
-Wuninitialized
-Wunknown-pragmas
-Wunused-function
-Wunused-label
-Wunused-value
-Wunused-variable
-Wvolatile-register-var
Note that some warning flags are not implied by -Wall. Some of
them warn about constructions that users generally do not consider
questionable, but which occasionally you might wish to check for;
others warn about constructions that are necessary or hard to avoid in
some cases, and there is no simple way to modify the code to suppress
the warning. Some of them are enabled by -Wextra but many of
them must be enabled individually.
-Wextra -Wclobbered
-Wempty-body
-Wignored-qualifiers
-Wmissing-field-initializers
-Wmissing-parameter-type (C only)
-Wold-style-declaration (C only)
-Woverride-init
-Wsign-compare
-Wtype-limits
-Wuninitialized
-Wunused-parameter (only with -Wunused or -Wall)
-Wunused-but-set-parameter (only with -Wunused or -Wall)
The option -Wextra also prints warning messages for the following cases:
-Wchar-subscriptschar. This is a common cause
of error, as programmers often forget that this type is signed on some
machines.
This warning is enabled by -Wall.
-Wcomment-Wno-cppSuppress warning messages emitted by #warning directives.
-Wdouble-promotion (C, C++, Objective-C and Objective-C++ only)float is implicitly
promoted to double. CPUs with a 32-bit “single-precision”
floating-point unit implement float in hardware, but emulate
double in software. On such a machine, doing computations
using double values is much more expensive because of the
overhead required for software emulation.
It is easy to accidentally do computations with double because
floating-point literals are implicitly of type double. For
example, in:
float area(float radius)
{
return 3.14159 * radius * radius;
}
the compiler will perform the entire computation with double
because the floating-point literal is a double.
-Wformatprintf and scanf, etc., to make sure that
the arguments supplied have types appropriate to the format string
specified, and that the conversions specified in the format string make
sense. This includes standard functions, and others specified by format
attributes (see Function Attributes), in the printf,
scanf, strftime and strfmon (an X/Open extension,
not in the C standard) families (or other target-specific families).
Which functions are checked without format attributes having been
specified depends on the standard version selected, and such checks of
functions without the attribute specified are disabled by
-ffreestanding or -fno-builtin.
The formats are checked against the format features supported by GNU
libc version 2.2. These include all ISO C90 and C99 features, as well
as features from the Single Unix Specification and some BSD and GNU
extensions. Other library implementations may not support all these
features; GCC does not support warning about features that go beyond a
particular library's limitations. However, if -pedantic is used
with -Wformat, warnings will be given about format features not
in the selected standard version (but not for strfmon formats,
since those are not in any version of the C standard). See Options Controlling C Dialect.
Since -Wformat also checks for null format arguments for several functions, -Wformat also implies -Wnonnull.
-Wformat is included in -Wall. For more control over some
aspects of format checking, the options -Wformat-y2k,
-Wno-format-extra-args, -Wno-format-zero-length,
-Wformat-nonliteral, -Wformat-security, and
-Wformat=2 are available, but are not included in -Wall.
-Wformat-y2kstrftime
formats which may yield only a two-digit year.
-Wno-format-contains-nul-Wno-format-extra-argsprintf or scanf format function. The C standard specifies
that such arguments are ignored.
Where the unused arguments lie between used arguments that are
specified with ‘$’ operand number specifications, normally
warnings are still given, since the implementation could not know what
type to pass to va_arg to skip the unused arguments. However,
in the case of scanf formats, this option will suppress the
warning if the unused arguments are all pointers, since the Single
Unix Specification says that such unused arguments are allowed.
-Wno-format-zero-length (C and Objective-C only)-Wformat-nonliteralva_list.
-Wformat-securityprintf and scanf functions where the
format string is not a string literal and there are no format arguments,
as in printf (foo);. This may be a security hole if the format
string came from untrusted input and contains ‘%n’. (This is
currently a subset of what -Wformat-nonliteral warns about, but
in future warnings may be added to -Wformat-security that are not
included in -Wformat-nonliteral.)
-Wformat=2-Wnonnull (C and Objective-C only)nonnull function attribute.
-Wnonnull is included in -Wall and -Wformat. It
can be disabled with the -Wno-nonnull option.
-Winit-self (C, C++, Objective-C and Objective-C++ only)For example, GCC will warn about i being uninitialized in the
following snippet only when -Winit-self has been specified:
int f()
{
int i = i;
return i;
}
-Wimplicit-int (C and Objective-C only)-Wimplicit-function-declaration (C and Objective-C only)-Wimplicit (C and Objective-C only)-Wignored-qualifiers (C and C++ only)const. For ISO C such a type qualifier has no effect,
since the value returned by a function is not an lvalue.
For C++, the warning is only emitted for scalar types or void.
ISO C prohibits qualified void return types on function
definitions, so such return types always receive a warning
even without this option.
This warning is also enabled by -Wextra.
-Wmain-Wmissing-braces int a[2][2] = { 0, 1, 2, 3 };
int b[2][2] = { { 0, 1 }, { 2, 3 } };
This warning is enabled by -Wall.
-Wmissing-include-dirs (C, C++, Objective-C and Objective-C++ only)-WparenthesesAlso warn if a comparison like ‘x<=y<=z’ appears; this is equivalent to ‘(x<=y ? 1 : 0) <= z’, which is a different interpretation from that of ordinary mathematical notation.
Also warn about constructions where there may be confusion to which
if statement an else branch belongs. Here is an example of
such a case:
{
if (a)
if (b)
foo ();
else
bar ();
}
In C/C++, every else branch belongs to the innermost possible
if statement, which in this example is if (b). This is
often not what the programmer expected, as illustrated in the above
example by indentation the programmer chose. When there is the
potential for this confusion, GCC will issue a warning when this flag
is specified. To eliminate the warning, add explicit braces around
the innermost if statement so there is no way the else
could belong to the enclosing if. The resulting code would
look like this:
{
if (a)
{
if (b)
foo ();
else
bar ();
}
}
Also warn for dangerous uses of the ?: with omitted middle operand GNU extension. When the condition in the ?: operator is a boolean expression the omitted value will be always 1. Often the user expects it to be a value computed inside the conditional expression instead.
This warning is enabled by -Wall.
-Wsequence-pointThe C and C++ standards defines the order in which expressions in a C/C++
program are evaluated in terms of sequence points, which represent
a partial ordering between the execution of parts of the program: those
executed before the sequence point, and those executed after it. These
occur after the evaluation of a full expression (one which is not part
of a larger expression), after the evaluation of the first operand of a
&&, ||, ? : or , (comma) operator, before a
function is called (but after the evaluation of its arguments and the
expression denoting the called function), and in certain other places.
Other than as expressed by the sequence point rules, the order of
evaluation of subexpressions of an expression is not specified. All
these rules describe only a partial order rather than a total order,
since, for example, if two functions are called within one expression
with no sequence point between them, the order in which the functions
are called is not specified. However, the standards committee have
ruled that function calls do not overlap.
It is not specified when between sequence points modifications to the values of objects take effect. Programs whose behavior depends on this have undefined behavior; the C and C++ standards specify that “Between the previous and next sequence point an object shall have its stored value modified at most once by the evaluation of an expression. Furthermore, the prior value shall be read only to determine the value to be stored.”. If a program breaks these rules, the results on any particular implementation are entirely unpredictable.
Examples of code with undefined behavior are a = a++;, a[n]
= b[n++] and a[i++] = i;. Some more complicated cases are not
diagnosed by this option, and it may give an occasional false positive
result, but in general it has been found fairly effective at detecting
this sort of problem in programs.
The standard is worded confusingly, therefore there is some debate over the precise meaning of the sequence point rules in subtle cases. Links to discussions of the problem, including proposed formal definitions, may be found on the GCC readings page, at http://gcc.gnu.org/readings.html.
This warning is enabled by -Wall for C and C++.
-Wreturn-typeint. Also warn about any return statement with no
return-value in a function whose return-type is not void
(falling off the end of the function body is considered returning
without a value), and about a return statement with an
expression in a function whose return-type is void.
For C++, a function without return type always produces a diagnostic message, even when -Wno-return-type is specified. The only exceptions are ‘main’ and functions defined in system headers.
This warning is enabled by -Wall.
-Wswitchswitch statement has an index of enumerated type
and lacks a case for one or more of the named codes of that
enumeration. (The presence of a default label prevents this
warning.) case labels outside the enumeration range also
provoke warnings when this option is used (even if there is a
default label).
This warning is enabled by -Wall.
-Wswitch-defaultswitch statement does not have a default
case.
-Wswitch-enumswitch statement has an index of enumerated type
and lacks a case for one or more of the named codes of that
enumeration. case labels outside the enumeration range also
provoke warnings when this option is used. The only difference
between -Wswitch and this option is that this option gives a
warning about an omitted enumeration code even if there is a
default label.
-Wsync-nand (C and C++ only)__sync_fetch_and_nand and __sync_nand_and_fetch
built-in functions are used. These functions changed semantics in GCC 4.4.
-Wtrigraphs-Wunused-but-set-parameterTo suppress this warning use the ‘unused’ attribute (see Variable Attributes).
This warning is also enabled by -Wunused together with
-Wextra.
-Wunused-but-set-variableTo suppress this warning use the ‘unused’ attribute (see Variable Attributes).
This warning is also enabled by -Wunused, which is enabled
by -Wall.
-Wunused-function-Wunused-labelTo suppress this warning use the ‘unused’ attribute
(see Variable Attributes).
-Wunused-parameterTo suppress this warning use the ‘unused’ attribute
(see Variable Attributes).
-Wno-unused-resultwarn_unused_result (see Variable Attributes) does not use
its return value. The default is -Wunused-result.
-Wunused-variableTo suppress this warning use the ‘unused’ attribute
(see Variable Attributes).
-Wunused-valueThis warning is enabled by -Wall.
-WunusedIn order to get a warning about an unused function parameter, you must
either specify ‘-Wextra -Wunused’ (note that ‘-Wall’ implies
‘-Wunused’), or separately specify -Wunused-parameter.
-Wuninitializedsetjmp call. In C++,
warn if a non-static reference or non-static ‘const’ member
appears in a class without constructors.
If you want to warn about code which uses the uninitialized value of the variable in its own initializer, use the -Winit-self option.
These warnings occur for individual uninitialized or clobbered
elements of structure, union or array variables as well as for
variables which are uninitialized or clobbered as a whole. They do
not occur for variables or elements declared volatile. Because
these warnings depend on optimization, the exact variables or elements
for which there are warnings will depend on the precise optimization
options and version of GCC used.
Note that there may be no warning about a variable that is used only to compute a value that itself is never used, because such computations may be deleted by data flow analysis before the warnings are printed.
These warnings are made optional because GCC is not smart enough to see all the reasons why the code might be correct despite appearing to have an error. Here is one example of how this can happen:
{
int x;
switch (y)
{
case 1: x = 1;
break;
case 2: x = 4;
break;
case 3: x = 5;
}
foo (x);
}
If the value of y is always 1, 2 or 3, then x is
always initialized, but GCC doesn't know this. Here is
another common case:
{
int save_y;
if (change_y) save_y = y, y = new_y;
...
if (change_y) y = save_y;
}
This has no bug because save_y is used only if it is set.
This option also warns when a non-volatile automatic variable might be
changed by a call to longjmp. These warnings as well are possible
only in optimizing compilation.
The compiler sees only the calls to setjmp. It cannot know
where longjmp will be called; in fact, a signal handler could
call it at any point in the code. As a result, you may get a warning
even when there is in fact no problem because longjmp cannot
in fact be called at the place which would cause a problem.
Some spurious warnings can be avoided if you declare all the functions
you use that never return as noreturn. See Function Attributes.
This warning is enabled by -Wall or -Wextra.
-Wunknown-pragmas-Wno-pragmas-Wstrict-aliasing-Wstrict-aliasing=nLevel 1: Most aggressive, quick, least accurate. Possibly useful when higher levels do not warn but -fstrict-aliasing still breaks the code, as it has very few false negatives. However, it has many false positives. Warns for all pointer conversions between possibly incompatible types, even if never dereferenced. Runs in the frontend only.
Level 2: Aggressive, quick, not too precise. May still have many false positives (not as many as level 1 though), and few false negatives (but possibly more than level 1). Unlike level 1, it only warns when an address is taken. Warns about incomplete types. Runs in the frontend only.
Level 3 (default for -Wstrict-aliasing):
Should have very few false positives and few false
negatives. Slightly slower than levels 1 or 2 when optimization is enabled.
Takes care of the common pun+dereference pattern in the frontend:
*(int*)&some_float.
If optimization is enabled, it also runs in the backend, where it deals
with multiple statement cases using flow-sensitive points-to information.
Only warns when the converted pointer is dereferenced.
Does not warn about incomplete types.
-Wstrict-overflow-Wstrict-overflow=nAn optimization which assumes that signed overflow does not occur is perfectly safe if the values of the variables involved are such that overflow never does, in fact, occur. Therefore this warning can easily give a false positive: a warning about code which is not actually a problem. To help focus on important issues, several warning levels are defined. No warnings are issued for the use of undefined signed overflow when estimating how many iterations a loop will require, in particular when determining whether a loop will be executed at all.
-Wstrict-overflow=1x + 1 > x; with -fstrict-overflow, the
compiler will simplify this to 1. This level of
-Wstrict-overflow is enabled by -Wall; higher levels
are not, and must be explicitly requested.
-Wstrict-overflow=2abs (x) >= 0. This can only be
simplified when -fstrict-overflow is in effect, because
abs (INT_MIN) overflows to INT_MIN, which is less than
zero. -Wstrict-overflow (with no level) is the same as
-Wstrict-overflow=2.
-Wstrict-overflow=3x + 1 > 1 will be simplified to x > 0.
-Wstrict-overflow=4(x * 10) / 5 will be simplified to x * 2.
-Wstrict-overflow=5x + 2 > y will
be simplified to x + 1 >= y. This is reported only at the
highest warning level because this simplification applies to many
comparisons, so this warning level will give a very large number of
false positives.
-Wsuggest-attribute=[pure|const|noreturn]-Wsuggest-attribute=pure-Wsuggest-attribute=const-Wsuggest-attribute=noreturnpure, const or noreturn. The compiler only warns for
functions visible in other compilation units or (in the case of pure and
const) if it cannot prove that the function returns normally. A function
returns normally if it doesn't contain an infinite loop nor returns abnormally
by throwing, calling abort() or trapping. This analysis requires option
-fipa-pure-const, which is enabled by default at -O and
higher. Higher optimization levels improve the accuracy of the analysis.
-Warray-bounds-Wno-div-by-zero-Wsystem-headers-WtrampolinesA trampoline is a small piece of data or code that is created at run
time on the stack when the address of a nested function is taken, and
is used to call the nested function indirectly. For some targets, it
is made up of data only and thus requires no special treatment. But,
for most targets, it is made up of code and thus requires the stack
to be made executable in order for the program to work properly.
-Wno-poison-system-directories-Wfloat-equalThe idea behind this is that sometimes it is convenient (for the
programmer) to consider floating-point values as approximations to
infinitely precise real numbers. If you are doing this, then you need
to compute (by analyzing the code, or in some other way) the maximum or
likely maximum error that the computation introduces, and allow for it
when performing comparisons (and when producing output, but that's a
different problem). In particular, instead of testing for equality, you
would check to see whether the two values have ranges that overlap; and
this is done with the relational operators, so equality comparisons are
probably mistaken.
-Wtraditional (C and Objective-C only)<limits.h>.
Use of these macros in user code might normally lead to spurious
warnings, however GCC's integrated preprocessor has enough context to
avoid warning in these cases.
switch statement has an operand of type long.
static function declaration follows a static one.
This construct is not accepted by some traditional C compilers.
__STDC__ to avoid missing
initializer warnings and relies on default initialization to zero in the
traditional C case.
PARAMS and
VPARAMS. This warning is also bypassed for nested functions
because that feature is already a GCC extension and thus not relevant to
traditional C compatibility.
-Wtraditional-conversion (C and Objective-C only)-Wdeclaration-after-statement (C and Objective-C only)-Wundef-Wno-endif-labels-Wshadow-Wlarger-than=len-Wframe-larger-than=lenalloca, variable-length arrays, or related constructs
is not included by the compiler when determining
whether or not to issue a warning.
-Wunsafe-loop-optimizations-Wno-pedantic-ms-format (MinGW targets only)printf / scanf format
width specifiers I32, I64, and I used on Windows targets
depending on the MS runtime, when you are using the options -Wformat
and -pedantic without gnu-extensions.
-Wpointer-arithvoid. GNU C assigns these types a size of 1, for
convenience in calculations with void * pointers and pointers
to functions. In C++, warn also when an arithmetic operation involves
NULL. This warning is also enabled by -pedantic.
-Wtype-limits-Wbad-function-cast (C and Objective-C only)int malloc() is cast to anything *.
-Wc++-compat (C and Objective-C only)void * to a pointer to non-void type.
-Wc++0x-compat (C++ and Objective-C++ only)-Wcast-qualconst char * is cast
to an ordinary char *.
Also warn when making a cast which introduces a type qualifier in an
unsafe way. For example, casting char ** to const char **
is unsafe, as in this example:
/* p is char ** value. */
const char **q = (const char **) p;
/* Assignment of readonly string to const char * is OK. */
*q = "string";
/* Now char** pointer points to read-only memory. */
**p = 'b';
-Wcast-alignchar * is cast to
an int * on machines where integers can only be accessed at
two- or four-byte boundaries.
-Wwrite-stringsconst
char[length] so that copying the address of one into a
non-const char * pointer will get a warning. These
warnings will help you find at compile time code that can try to write
into a string constant, but only if you have been very careful about
using const in declarations and prototypes. Otherwise, it will
just be a nuisance. This is why we did not make -Wall request
these warnings.
When compiling C++, warn about the deprecated conversion from string
literals to char *. This warning is enabled by default for C++
programs.
-Wclobbered-Wconversionabs (x) when
x is double; conversions between signed and unsigned,
like unsigned ui = -1; and conversions to smaller types, like
sqrtf (M_PI). Do not warn for explicit casts like abs
((int) x) and ui = (unsigned) -1, or if the value is not
changed by the conversion like in abs (2.0). Warnings about
conversions between signed and unsigned integers can be disabled by
using -Wno-sign-conversion.
For C++, also warn for confusing overload resolution for user-defined
conversions; and conversions that will never use a type conversion
operator: conversions to void, the same type, a base class or a
reference to them. Warnings about conversions between signed and
unsigned integers are disabled by default in C++ unless
-Wsign-conversion is explicitly enabled.
-Wno-conversion-null (C++ and Objective-C++ only)NULL and non-pointer
types. -Wconversion-null is enabled by default.
-Wempty-body-Wenum-compare-Wjump-misses-init (C, Objective-C only)goto statement or a switch statement jumps
forward across the initialization of a variable, or jumps backward to a
label after the variable has been initialized. This only warns about
variables which are initialized when they are declared. This warning is
only supported for C and Objective C; in C++ this sort of branch is an
error in any case.
-Wjump-misses-init is included in -Wc++-compat. It
can be disabled with the -Wno-jump-misses-init option.
-Wsign-compare-Wsign-conversion-Waddressvoid func(void); if (func), and comparisons against the memory
address of a string literal, such as if (x == "abc"). Such
uses typically indicate a programmer error: the address of a function
always evaluates to true, so their use in a conditional usually
indicate that the programmer forgot the parentheses in a function
call; and comparisons against string literals result in unspecified
behavior and are not portable in C, so they usually indicate that the
programmer intended to use strcmp. This warning is enabled by
-Wall.
-Wlogical-op-Waggregate-return-Wno-attributes__attribute__ is used, such as
unrecognized attributes, function attributes applied to variables,
etc. This will not stop errors for incorrect use of supported
attributes.
-Wno-builtin-macro-redefined__TIMESTAMP__, __TIME__,
__DATE__, __FILE__, and __BASE_FILE__.
-Wstrict-prototypes (C and Objective-C only)-Wold-style-declaration (C and Objective-C only)static are not the first things in a declaration. This warning
is also enabled by -Wextra.
-Wold-style-definition (C and Objective-C only)-Wmissing-parameter-type (C and Objective-C only) void foo(bar) { }
This warning is also enabled by -Wextra.
-Wmissing-prototypes (C and Objective-C only)-Wmissing-declarations-Wmissing-field-initializersx.h is implicitly zero:
struct s { int f, g, h; };
struct s x = { 3, 4 };
This option does not warn about designated initializers, so the following modification would not trigger a warning:
struct s { int f, g, h; };
struct s x = { .f = 3, .g = 4 };
This warning is included in -Wextra. To get other -Wextra
warnings without this one, use ‘-Wextra -Wno-missing-field-initializers’.
-Wmissing-format-attributeformat
attributes. Note these are only possible candidates, not absolute ones.
GCC will guess that function pointers with format attributes that
are used in assignment, initialization, parameter passing or return
statements should have a corresponding format attribute in the
resulting type. I.e. the left-hand side of the assignment or
initialization, the type of the parameter variable, or the return type
of the containing function respectively should also have a format
attribute to avoid the warning.
GCC will also warn about function definitions which might be
candidates for format attributes. Again, these are only
possible candidates. GCC will guess that format attributes
might be appropriate for any function that calls a function like
vprintf or vscanf, but this might not always be the
case, and some functions for which format attributes are
appropriate may not be detected.
-Wno-multichar-Wnormalized=<none|id|nfc|nfkc>There are four levels of warning that GCC supports. The default is -Wnormalized=nfc, which warns about any identifier which is not in the ISO 10646 “C” normalized form, NFC. NFC is the recommended form for most uses.
Unfortunately, there are some characters which ISO C and ISO C++ allow in identifiers that when turned into NFC aren't allowable as identifiers. That is, there's no way to use these symbols in portable ISO C or C++ and have all your identifiers in NFC. -Wnormalized=id suppresses the warning for these characters. It is hoped that future versions of the standards involved will correct this, which is why this option is not the default.
You can switch the warning off for all characters by writing -Wnormalized=none. You would only want to do this if you were using some other normalization scheme (like “D”), because otherwise you can easily create bugs that are literally impossible to see.
Some characters in ISO 10646 have distinct meanings but look identical
in some fonts or display methodologies, especially once formatting has
been applied. For instance \u207F, “SUPERSCRIPT LATIN SMALL
LETTER N”, will display just like a regular n which has been
placed in a superscript. ISO 10646 defines the NFKC
normalization scheme to convert all these into a standard form as
well, and GCC will warn if your code is not in NFKC if you use
-Wnormalized=nfkc. This warning is comparable to warning
about every identifier that contains the letter O because it might be
confused with the digit 0, and so is not the default, but may be
useful as a local coding convention if the programming environment is
unable to be fixed to display these characters distinctly.
-Wno-deprecated-Wno-deprecated-declarationsdeprecated
attribute.
-Wno-overflow-Woverride-init (C and Objective-C only)This warning is included in -Wextra. To get other
-Wextra warnings without this one, use ‘-Wextra
-Wno-override-init’.
-Wpackedf.x in struct bar
will be misaligned even though struct bar does not itself
have the packed attribute:
struct foo {
int x;
char a, b, c, d;
} __attribute__((packed));
struct bar {
char z;
struct foo f;
};
-Wpacked-bitfield-compatpacked attribute
on bit-fields of type char. This has been fixed in GCC 4.4 but
the change can lead to differences in the structure layout. GCC
informs you when the offset of such a field has changed in GCC 4.4.
For example there is no longer a 4-bit padding between field a
and b in this structure:
struct foo
{
char a:4;
char b:8;
} __attribute__ ((packed));
This warning is enabled by default. Use
-Wno-packed-bitfield-compat to disable this warning.
-Wpadded-Wredundant-decls-Wnested-externs (C and Objective-C only)extern declaration is encountered within a function.
-WinlineThe compiler uses a variety of heuristics to determine whether or not
to inline a function. For example, the compiler takes into account
the size of the function being inlined and the amount of inlining
that has already been done in the current function. Therefore,
seemingly insignificant changes in the source program can cause the
warnings produced by -Winline to appear or disappear.
-Wno-invalid-offsetof (C++ and Objective-C++ only)The restrictions on ‘offsetof’ may be relaxed in a future version
of the C++ standard.
-Wno-int-to-pointer-cast-Wno-pointer-to-int-cast (C and Objective-C only)-Winvalid-pch-Wlong-long-Wvariadic-macros-Wvla-Wvolatile-register-var-Wdisabled-optimization-Wpointer-sign (C and Objective-C only)-Wstack-protector-Wno-mudflap-Woverlength-stringsThe limit applies after string constant concatenation, and does not count the trailing NUL. In C90, the limit was 509 characters; in C99, it was raised to 4095. C++98 does not specify a normative minimum maximum, so we do not diagnose overlength strings in C++.
This option is implied by -pedantic, and can be disabled with
-Wno-overlength-strings.
-Wunsuffixed-float-constants (C and Objective-C only)FLOAT_CONST_DECIMAL64 pragma
from the decimal floating-point extension to C99.